UF_CUT_LEVEL_single_s
(view source)
Defined in: uf_cut_levels.h
Also known as:
UF_CUT_LEVEL_single_t
Overview
Data structure for a single cut level.
Data Members
entity_tag
tag_t
Tag id of the face or point entity
used to define the current cut level.
This can be NULL if the level was
defined by an explicit z level.
z_level
double
The z distance of the cut level from the
origin along the normal of the cut levels.
local_cut_depth
double
The max depth per cut value to be
used for the range between this cut
level and the one above it.
used to define the current cut level.
This can be NULL if the level was
defined by an explicit z level.