UF_CUTTER_tracking_point_data_s (view source)
 
Defined in: uf_cutter.h
 
Also known as:
 
Overview
tracking point data structure for a Milling Cutter tracking point


Data Members

diameter
double
The output diameter of the point

distance
double
The distance of the point along the tool axis

zoff
double
The postprocessor Z offset of the point

adjust
int
The adjust register to use with this point

cutcom
int
The cutcom register to use with this point

zoff_status
int
The active/inactive status of the Z offset

adjust_status
int
The active/inactive status of the adjust register

cutcom_status
int
The active/inactive status of the cutcom register

name [ UF_OBJ_NAME_BUFSIZE ]
char
The name of the tracking point