UF_CAM_preferences_s (view source)
Defined in: uf_cam.h
Also known as:
- UF_CAM_preferences_t
- UF_CAM_preferences_p_t
Overview
NOTES on UF_CAM_preferences_t:
1) all items that refer to color can take any of the color values that
appear in uf_obj.h.
2) all the item here have the same meaning as defined in the CAM
Preferences chapter of the NX Users Manual.
Data Members
blank_geom_color
int
blank_geom_type
int
check_geom_color
int
check_geom_type
int
clearance_geom_color
int
clsf_decimal_place
int
clsf_replay_advanced
clsf_replay_refresh
clsf_replay_vericut
clsf_type
int
collect_instances
create_tool_lib_entry
cut_area_geom_color
int
cut_area_geom_type
int
delete_param_set
drive_geom_color
int
generate_instance
info_csys
int
macro_only
mcs_link_to_rcs
int
mcs_stat
int
parent_display
part_geom_color
int
part_geom_type
int
pause_aft_path
rcs_disp_stat
int
rcs_inv_matrix [ 9 ]
double
rcs_map_stat
int
rcs_origin [ 3 ]
double
rcs_stat
int
refresh_bef_path
show_edited_status
show_standard_type
show_template_type
show_tool_name
template_tool
toolpath_only
template_set_used [ UF_CAM_MAX_TEMPLATE_SET_NAME_BUFSIZE ]
char
transform_toolpath
trim_geom_color
int
uncut_geom_color
int
unlink_instance
use_customized_interface
visible_scrollable_items
int
automatically_update_when_loading