UF_BREP_plane_s (view source)
Defined in: uf_brep_types.h
Also known as:
- UF_BREP_plane_t
- UF_BREP_plane_p_t
Overview
Contains data representing a plane. The u parameter is along the reference
direction and the v parameter is at right angles to it, which places the
plane in the x-y plane of a right handed coordinate system with the
reference direction as the x axis and the normal vector as the z axis.
Parameter values are in part units.
Data Members
pt_on_plane [ 3 ]
double
normal [ 3 ]
double
u0_ref_direc [ 3 ]
double