UI Name | Automation (neutral) Name | Value type | Range | Default Value | |||||
---|---|---|---|---|---|---|---|---|---|
Scratch Directory | ScratchDir | string | -- | -- | |||||
Task Entry | TaskEntry | integer |
|
0 | |||||
Memory Allocation Options | memory parameters | integer |
|
2 | |||||
Percentage Limit (%) see note (1) |
percentage memory | integer | 0to 0 | 50 | |||||
Maximum Amount in Units of Megabytes see note (2) |
Memory | integer | 0to 0 | CAE_DefaultAbaqusSolverMemory | |||||
Maximum Amount in Units of Gigabytes see note (3) |
Memory GB | integer | 0to 0 | 1 | |||||
Parallel Processing | parallelization | boolean | true or false | true | |||||
Number of Processors (cpus) see note (4) |
nprocessors | integer | 1to 1 | 2 | |||||
Parallelization Method see note (5) |
pmethod | integer |
|
0 | |||||
Nodal Field Output Precision | outputprecision | integer |
|
0 | |||||
Use environment variable UGII_ABAQUS | ugii_abaqus | boolean | true or false | CAE_DefaultAbaqusSolverEnv | |||||
User Specified see note (6) |
solver executable | string | -- | CAE_DefaultAbaqusSolverLocation | |||||
Write out group data | write group data | boolean | true or false | false |