Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldTaperMethod |
WeldTaperMethod.FROM_END_FACE
Taper will be measured from groove end caps
|
static WeldTaperMethod |
WeldTaperMethod.FROM_SIDE_FACE
Taper will be measured from groove side face
|
Modifier and Type | Method and Description |
---|---|
WeldTaperMethod |
GrooveBuilder.taperMethod()
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.taperMethod() and WeldGrooveBuilder.setTaperMethod(nxopen.weld.WeldGrooveBuilder.Taper) instead.
|
static WeldTaperMethod |
WeldTaperMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldTaperMethod |
WeldTaperMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldTaperMethod[] |
WeldTaperMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GrooveBuilder.setTaperMethod(WeldTaperMethod taperMethod)
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.taperMethod() and WeldGrooveBuilder.setTaperMethod(nxopen.weld.WeldGrooveBuilder.Taper) instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.