Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldPointSpacingMethod |
WeldPointSpacingMethod.DISTANCE
Place multiple spot welds based on distance
|
static WeldPointSpacingMethod |
WeldPointSpacingMethod.NUM_POINTS
Place multiple spot welds based on number of points
|
Modifier and Type | Method and Description |
---|---|
WeldPointSpacingMethod |
WeldPointBuilder.referenceSheetSpacingMethod()
Returns the refsheet spacing method
License requirements: ugweld ("UG WELD") . |
static WeldPointSpacingMethod |
WeldPointSpacingMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointSpacingMethod |
WeldPointSpacingMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointSpacingMethod[] |
WeldPointSpacingMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldPointBuilder.setReferenceSheetSpacingMethod(WeldPointSpacingMethod spacingMethod)
Sets the refsheet spacing method
License requirements: ugweld ("UG WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.