Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldPointMethod |
WeldPointMethod.FROM_POINTS
create fix/single/none points using existing points
|
static WeldPointMethod |
WeldPointMethod.MIRROR
mirror existing points
|
static WeldPointMethod |
WeldPointMethod.MULTIPLE
use guide curve(s) or edge(s) to generate spot weld points
|
static WeldPointMethod |
WeldPointMethod.SINGLE
use point constructor to generate spot weld points
|
static WeldPointMethod |
WeldPointMethod.TRANSLATE
translate existing points
|
Modifier and Type | Method and Description |
---|---|
WeldPointMethod |
WeldPointBuilder.pointMethod()
Returns the method for creating weld points.
|
static WeldPointMethod |
WeldPointMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointMethod |
WeldPointMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointMethod[] |
WeldPointMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldPointBuilder.setPointMethod(WeldPointMethod ptMethod)
License requirements: ugweld ("UG WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.