Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.GUIDE_CURVE
Feature was created using the guide curves method.
|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.GUIDE_CURVE_MOVED_OFF
Feature was created using the guide curves method, but user moved it off.
|
WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.FeatureInfo.methodUsed
the method used to create the feature
|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.MIRROR
Feature was created using the mirror method.
|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.NONE
No method specified.
|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.POINTS
Feature was created using the points method.
|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.TRANSLATE
Feature was created using the translate method.
|
Modifier and Type | Method and Description |
---|---|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointExitBuilder.MethodUsed |
WeldPointExitBuilder.MethodUsed.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointExitBuilder.MethodUsed[] |
WeldPointExitBuilder.MethodUsed.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
FeatureInfo(nxopen.features.Feature featureInitial,
WeldPointExitBuilder.MethodUsed methodUsedInitial,
nxopen.features.Feature parentInitial,
boolean isNewlyCreatedInitial)
Constructor for the FeatureInfo object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.