Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.DATUM_LOCATOR
Datum Locator command
|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.JOINTMARK
Joint Mark command
|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.MEASUREMENT_LOCATOR
Measurement Locator command
|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.NONE
No command.
|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.WELD_POINT
Weld Point command
|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.WELD_POINT_WIZARD
Weld Point Wizard command
|
Modifier and Type | Method and Description |
---|---|
WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.commandUsed()
Returns the command name that was last used to create features.
|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldPointExitBuilder.CommandName |
WeldPointExitBuilder.CommandName.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldPointExitBuilder.CommandName[] |
WeldPointExitBuilder.CommandName.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.