Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldGrooveType |
WeldGrooveType.EDGES_NOT_PREPARED
Edges are not prepared
|
static WeldGrooveType |
WeldGrooveType.EDGES_PREPARED
Edges are prepared
|
Modifier and Type | Method and Description |
---|---|
WeldGrooveType |
GrooveBuilder.grooveType()
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.edgeType() and WeldGrooveBuilder.setEdgeType(nxopen.weld.WeldGrooveBuilder.Edge) instead.
|
static WeldGrooveType |
WeldGrooveType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldGrooveType |
WeldGrooveType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldGrooveType[] |
WeldGrooveType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GrooveBuilder.setGrooveType(WeldGrooveType grooveType)
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.edgeType() and WeldGrooveBuilder.setEdgeType(nxopen.weld.WeldGrooveBuilder.Edge) instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.