Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldFillBuilder.BoundaryMethodType |
WeldFillBuilder.BoundaryMethodType.CURVE
Boundary defined by a curve.
|
static WeldFillBuilder.BoundaryMethodType |
WeldFillBuilder.BoundaryMethodType.RECTANGLE
Boundary defined by a two point rectangle.
|
Modifier and Type | Method and Description |
---|---|
WeldFillBuilder.BoundaryMethodType |
WeldFillBuilder.boundaryMethod()
Returns the type of boundary to create the fill from.
|
static WeldFillBuilder.BoundaryMethodType |
WeldFillBuilder.BoundaryMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldFillBuilder.BoundaryMethodType |
WeldFillBuilder.BoundaryMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldFillBuilder.BoundaryMethodType[] |
WeldFillBuilder.BoundaryMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldFillBuilder.setBoundaryMethod(WeldFillBuilder.BoundaryMethodType boundaryMethod)
License requirements: ugweld ("UG WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.