Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static OutputType |
OutputType.ASSOCIATIVE
output data will be associated to inputs.
|
static OutputType |
OutputType.FIXED
output data will not change if inputs change
|
Modifier and Type | Method and Description |
---|---|
OutputType |
WeldPointBuilder.outputType()
Returns the output type.
|
OutputType |
GrooveBuilder.outputType()
Deprecated.
Deprecated in NX9.0.0. This functionality is no longer supported.
|
static OutputType |
OutputType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OutputType |
OutputType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OutputType[] |
OutputType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldPointBuilder.setOutputType(OutputType outputType)
Sets the output type.
|
void |
GrooveBuilder.setOutputType(OutputType outputType)
Deprecated.
Deprecated in NX9.0.0. This functionality is no longer supported.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.