Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static InformationBuilder.AttributeOriginType |
InformationBuilder.AttributeOriginType.DF |
static InformationBuilder.AttributeOriginType |
InformationBuilder.AttributeOriginType.OBJECT |
Modifier and Type | Method and Description |
---|---|
InformationBuilder.AttributeOriginType |
InformationBuilder.attributeOrigin()
Returns the option indicating where the attributes are read from, welding object or corresponding Design Feature.
|
static InformationBuilder.AttributeOriginType |
InformationBuilder.AttributeOriginType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InformationBuilder.AttributeOriginType |
InformationBuilder.AttributeOriginType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InformationBuilder.AttributeOriginType[] |
InformationBuilder.AttributeOriginType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InformationBuilder.setAttributeOrigin(InformationBuilder.AttributeOriginType attributeOrigin)
License requirements: ugweld ("UG WELD") OR structure_weld ("STRUCTURE WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.