Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static EdgePrepValuesBuilder.Apply |
EdgePrepValuesBuilder.Apply.TO_ALL_VALUES
Update all values of each selected joint.
|
static EdgePrepValuesBuilder.Apply |
EdgePrepValuesBuilder.Apply.TO_CHANGED_VALUES_ONLY
Update only the changed values to each selected joint.
|
Modifier and Type | Method and Description |
---|---|
static EdgePrepValuesBuilder.Apply |
EdgePrepValuesBuilder.Apply.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgePrepValuesBuilder.Apply |
EdgePrepValuesBuilder.Apply.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgePrepValuesBuilder.Apply[] |
EdgePrepValuesBuilder.Apply.values()
Returns an array that contains the values for this enum.
|
EdgePrepValuesBuilder.Apply |
EdgePrepValuesBuilder.valuesApplyOption()
Returns the apply values option which indicates whether the all the values of each selected joint should be updated or just the values that were changed in the
JointExitBuilder . |
Modifier and Type | Method and Description |
---|---|
void |
EdgePrepValuesBuilder.setValuesApplyOption(EdgePrepValuesBuilder.Apply option)
License requirements: structure_weld ("STRUCTURE WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.