Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static EasyPatternBuilder.HemMethodTypes |
EasyPatternBuilder.HemMethodTypes.MID_POINT
Use the mid point of a section cut.
|
static EasyPatternBuilder.HemMethodTypes |
EasyPatternBuilder.HemMethodTypes.NORMAL_TO_BODY
Use Normal to Body Method.
|
Modifier and Type | Method and Description |
---|---|
EasyPatternBuilder.HemMethodTypes |
EasyPatternBuilder.hemMethod()
Returns the hem method.
|
static EasyPatternBuilder.HemMethodTypes |
EasyPatternBuilder.HemMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EasyPatternBuilder.HemMethodTypes |
EasyPatternBuilder.HemMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EasyPatternBuilder.HemMethodTypes[] |
EasyPatternBuilder.HemMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EasyPatternBuilder.setHemMethod(EasyPatternBuilder.HemMethodTypes hemMethod)
License requirements: ugweld ("UG WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.