Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.CUSTOM1
A datum surface or pin specified in the customer defaults by the Custom1 type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.CUSTOM2
A datum surface or pin specified in the customer defaults by the Custom2 type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.CUSTOM3
A datum surface or pin specified in the customer defaults by the Custom3 type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.CUSTOM4
A datum surface or pin specified in the customer defaults by the Custom4 type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.CUSTOM5
A datum surface or pin specified in the customer defaults by the Custom5 type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.CUSTOM6
A datum surface or pin specified in the customer defaults by the Custom6 type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.CUSTOM7
A datum surface or pin specified in the customer defaults by the Custom7 type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.DEFAULT
A datum surface or pin specified in the customer defaults by the Default type.
|
Modifier and Type | Method and Description |
---|---|
DatumCommonBuilder.CustomTypes |
DatumIconBuilder.customType()
Returns the custom datum type from the customer defaults that was used.
|
DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.customType()
Returns the custom datum type.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumCommonBuilder.CustomTypes |
DatumCommonBuilder.CustomTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumCommonBuilder.CustomTypes[] |
DatumCommonBuilder.CustomTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumCommonBuilder.setCustomType(DatumCommonBuilder.CustomTypes customType)
License requirements: ugweld ("UG WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.