public static class WeldJointBuilder.CoordinateSystem extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ABSOLUTE
Desired points and vectors should be in absolute coordinates.
|
static int |
_SHIP
Desired points and vectors should be in ship coordinate system.
|
static WeldJointBuilder.CoordinateSystem |
ABSOLUTE
Desired points and vectors should be in absolute coordinates.
|
static WeldJointBuilder.CoordinateSystem |
SHIP
Desired points and vectors should be in ship coordinate system.
|
Modifier and Type | Method and Description |
---|---|
static WeldJointBuilder.CoordinateSystem |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldJointBuilder.CoordinateSystem |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldJointBuilder.CoordinateSystem[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldJointBuilder.CoordinateSystem ABSOLUTE
public static final WeldJointBuilder.CoordinateSystem SHIP
public static final int _ABSOLUTE
public static final int _SHIP
public static WeldJointBuilder.CoordinateSystem valueOf(int value)
public static WeldJointBuilder.CoordinateSystem valueOf(String name)
public static WeldJointBuilder.CoordinateSystem[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.