public static class WeldFillBuilder.WidthAlongType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_XC
The length is aligned along the current WCS X direction.
|
static int |
_YC
The length is aligned along the current WCS Y direction.
|
static WeldFillBuilder.WidthAlongType |
XC
The length is aligned along the current WCS X direction.
|
static WeldFillBuilder.WidthAlongType |
YC
The length is aligned along the current WCS Y direction.
|
Modifier and Type | Method and Description |
---|---|
static WeldFillBuilder.WidthAlongType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldFillBuilder.WidthAlongType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldFillBuilder.WidthAlongType[] |
values()
Returns an array that contains the values for this enum.
|
public static final WeldFillBuilder.WidthAlongType XC
public static final WeldFillBuilder.WidthAlongType YC
public static final int _XC
public static final int _YC
public static WeldFillBuilder.WidthAlongType valueOf(int value)
public static WeldFillBuilder.WidthAlongType valueOf(String name)
public static WeldFillBuilder.WidthAlongType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.