public interface PointMarkBuilder extends JointmarkBuilder
PointMark
feature. WeldManager.createPointMarkBuilder(nxopen.weld.PointMark)
Property | Value |
---|---|
Associativity | 1 |
ConnectPart | 0 |
ConstructionMethod | GuideCurve |
CreateSingleFeatures | 0 |
DistanceTolerance | 0.0254 |
OrientationMethod | SurfaceNormal |
ReferenceSheetType | Overlap |
ShowWorkCsys | 1 |
Modifier and Type | Interface and Description |
---|---|
static class |
PointMarkBuilder.WeldTypes
The weld type to create.
|
JointmarkBuilder.ConnectedPanelTypes, JointmarkBuilder.Method, JointmarkBuilder.OrientationMethodTypes, JointmarkBuilder.ReferenceSheetTypes
Modifier and Type | Method and Description |
---|---|
void |
appendPointsOverride(boolean create)
Creates a list of points on the overlap sheet.
|
PointMarkPointBuilder |
newPointsOverride()
Creates a
PointMarkPointBuilder object. |
void |
setShowSolids(boolean showSolids)
License requirements: ugweld ("UG WELD") . |
void |
setWeldType(PointMarkBuilder.WeldTypes weldType)
License requirements: ugweld ("UG WELD") . |
boolean |
showSolids()
Returns the display mode.
|
PointMarkBuilder.WeldTypes |
weldType()
Returns the weld type references in the customer defaults to create.
|
appendPoints, associativity, characteristics, connectedPanelType, connectPart, constructionMethod, createReferenceData, createSingleFeatures, createSymbolCurve, deleteReferenceData, distanceTolerance, faceSetsList, fixedCsys, getReferenceSheet, getSelectedReferences, getSheetEdges, guideCurvesList, mapFeaturesToPoints, newFaceSets, newGuide, newPoints, orientationMethod, plane, pointList, rediscoverFaces, referenceSheetType, reuseFeatures, selectMirrorObject, selectPointsObject, selectTranslateObject, setAssociativity, setConnectedPanelType, setConnectPart, setConstructionMethod, setCreateSingleFeatures, setDisplayCsys, setDistanceTolerance, setFixedCsys, setOrientationMethod, setPlane, setReferenceSheetType, setShowThruState, setShowWorkCsys, setTranslateCsys, setVector, showWorkCsys, translateCsys, translateX, translateY, translateZ, updateFeatures, updateReferenceSheet, vector
PointMarkBuilder.WeldTypes weldType() throws NXException, RemoteException
NXException
RemoteException
void setWeldType(PointMarkBuilder.WeldTypes weldType) throws NXException, RemoteException
weldType
- NXException
RemoteException
PointMarkPointBuilder newPointsOverride() throws NXException, RemoteException
PointMarkPointBuilder
object.
NXException
RemoteException
void appendPointsOverride(boolean create) throws NXException, RemoteException
create
- Create or EditNXException
RemoteException
boolean showSolids() throws NXException, RemoteException
NXException
RemoteException
void setShowSolids(boolean showSolids) throws NXException, RemoteException
showSolids
- true- Show Weld.PointMarkPoint features in solid mode. fale- show in point mode.NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.