public static class EasyPatternBuilder.HemMethodTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MID_POINT
Use the mid point of a section cut.
|
static int |
_NORMAL_TO_BODY
Use Normal to Body Method.
|
static EasyPatternBuilder.HemMethodTypes |
MID_POINT
Use the mid point of a section cut.
|
static EasyPatternBuilder.HemMethodTypes |
NORMAL_TO_BODY
Use Normal to Body Method.
|
Modifier and Type | Method and Description |
---|---|
static EasyPatternBuilder.HemMethodTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EasyPatternBuilder.HemMethodTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EasyPatternBuilder.HemMethodTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final EasyPatternBuilder.HemMethodTypes MID_POINT
public static final EasyPatternBuilder.HemMethodTypes NORMAL_TO_BODY
public static final int _MID_POINT
public static final int _NORMAL_TO_BODY
public static EasyPatternBuilder.HemMethodTypes valueOf(int value)
public static EasyPatternBuilder.HemMethodTypes valueOf(String name)
public static EasyPatternBuilder.HemMethodTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.