public static class VisualReportExplorer.ReportOnObjectsOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD
Add to the existing set of objects
|
static int |
_REPLACE
Replace the existing set of objects
|
static VisualReportExplorer.ReportOnObjectsOption |
ADD
Add to the existing set of objects
|
static VisualReportExplorer.ReportOnObjectsOption |
REPLACE
Replace the existing set of objects
|
Modifier and Type | Method and Description |
---|---|
static VisualReportExplorer.ReportOnObjectsOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VisualReportExplorer.ReportOnObjectsOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VisualReportExplorer.ReportOnObjectsOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final VisualReportExplorer.ReportOnObjectsOption REPLACE
public static final VisualReportExplorer.ReportOnObjectsOption ADD
public static final int _REPLACE
public static final int _ADD
public static VisualReportExplorer.ReportOnObjectsOption valueOf(int value)
public static VisualReportExplorer.ReportOnObjectsOption valueOf(String name)
public static VisualReportExplorer.ReportOnObjectsOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.