Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Class and Description |
---|
RequirementCheckCollection
Represents an NX
RequirementCheckCollection object. |
RequirementCollection
Represents an NX
RequirementCollection object. |
ValidationManager
Represents an object that manages validator and parser associated instance objects.
|
XmlComparator
Provides a generic comparator for finding differences between two XML
format files.
|
Class and Description |
---|
Override
Represents a
Override object. |
OverrideBuilder
Represents a
Override builder To create a new instance of this class, use ResultObject.createOverrideBuilder(nxopen.validate.Override) Default values. |
OverrideBuilder.DecisionActions
Represents the override request decision action
|
OverrideBuilder.RequestTypes
Represents the override request type
|
OverrideBuilder.ToStates
Represents the override request to state
|
Parser
Represents a NX
Parser . |
Parser.DataSourceTypes
The data source type of check result.
|
Requirement
Represents a
Requirement object. |
RequirementBuilder
Represents a
Requirement builder To create a new instance of this class, use RequirementCollection.createRequirementBuilder(nxopen.validate.Requirement) Default values. |
RequirementBuilder.DataTypeOptions
This enum represents the data type of the value in requirement
|
RequirementBuilder.DefinitionMethodOptions
This enum represents the type of requirement definition method
|
RequirementBuilder.RelationalOperatorOptions
This enum represents the relational operator for comparing values
|
RequirementBuilder.SeverityOptions
This enum represents the severity level when a requirement is not satisfied
|
RequirementCheck
Represents an NX
RequirementCheck object. |
RequirementCheck.SaveResultsToTeamcenterOptions
This enum represents the Save Results to Teamcenter option
|
RequirementCollection.SourceTypeOptions
This enum represents the type of external source where requirement is defined
|
ResultObject
Represents a check-mate result object.
|
ResultObject.ResultTypes
The type of check result
|
Validator
Represents a NX
Validator . |
ValidatorOptions
Contains information about run options of check-mate checking process.
|
ValidatorOptions.LogModeTypes
The log mode type.
|
ValidatorOptions.ResultsDisplayModeTypes
The results display mode type.
|
ValidatorOptions.SaveModeTypes
The save mode type.
|
XmlComparator.Options
Represents config options in comparison For example: case 1: Defines filter file to control what nodes will be compared; generates comparison report and log; ignores CDATA and processing instruction nodes. |
XmlComparator.Result
Specifies result of the comparison
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.