public static class UserDefinedObject.LinkStatus extends Enum
nxopen.features.UserDefinedObjectFeature
Modifier and Type | Field and Description |
---|---|
static int |
_OUT_OF_DATE
The associated object is out of date.
|
static int |
_UP_TO_DATE
The associated object is up to date.
|
static UserDefinedObject.LinkStatus |
OUT_OF_DATE
The associated object is out of date.
|
static UserDefinedObject.LinkStatus |
UP_TO_DATE
The associated object is up to date.
|
Modifier and Type | Method and Description |
---|---|
static UserDefinedObject.LinkStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UserDefinedObject.LinkStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UserDefinedObject.LinkStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final UserDefinedObject.LinkStatus UP_TO_DATE
public static final UserDefinedObject.LinkStatus OUT_OF_DATE
public static final int _UP_TO_DATE
public static final int _OUT_OF_DATE
public static UserDefinedObject.LinkStatus valueOf(int value)
public static UserDefinedObject.LinkStatus valueOf(String name)
public static UserDefinedObject.LinkStatus[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.