public static class ValidCheckBuilder.AnalysisMode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FACET_BASED
Facet body will be used to do checking
|
static int |
_SOLID_BASED
Solid body will be used to do checking
|
static ValidCheckBuilder.AnalysisMode |
FACET_BASED
Facet body will be used to do checking
|
static ValidCheckBuilder.AnalysisMode |
SOLID_BASED
Solid body will be used to do checking
|
Modifier and Type | Method and Description |
---|---|
static ValidCheckBuilder.AnalysisMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ValidCheckBuilder.AnalysisMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ValidCheckBuilder.AnalysisMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final ValidCheckBuilder.AnalysisMode SOLID_BASED
public static final ValidCheckBuilder.AnalysisMode FACET_BASED
public static final int _SOLID_BASED
public static final int _FACET_BASED
public static ValidCheckBuilder.AnalysisMode valueOf(int value)
public static ValidCheckBuilder.AnalysisMode valueOf(String name)
public static ValidCheckBuilder.AnalysisMode[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.