public static class PiercingInsertBuilder.PunchPocketTypeItemsPP extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CIRCLE
Punch pocket type in punch plate is circle
|
static int |
_CLEARANCE
Punch pocket type in punch plate is clearance
|
static int |
_FILLET
Punch pocket type in punch plate is fillet
|
static PiercingInsertBuilder.PunchPocketTypeItemsPP |
CIRCLE
Punch pocket type in punch plate is circle
|
static PiercingInsertBuilder.PunchPocketTypeItemsPP |
CLEARANCE
Punch pocket type in punch plate is clearance
|
static PiercingInsertBuilder.PunchPocketTypeItemsPP |
FILLET
Punch pocket type in punch plate is fillet
|
Modifier and Type | Method and Description |
---|---|
static PiercingInsertBuilder.PunchPocketTypeItemsPP |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PiercingInsertBuilder.PunchPocketTypeItemsPP |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PiercingInsertBuilder.PunchPocketTypeItemsPP[] |
values()
Returns an array that contains the values for this enum.
|
public static final PiercingInsertBuilder.PunchPocketTypeItemsPP CLEARANCE
public static final PiercingInsertBuilder.PunchPocketTypeItemsPP FILLET
public static final PiercingInsertBuilder.PunchPocketTypeItemsPP CIRCLE
public static final int _CLEARANCE
public static final int _FILLET
public static final int _CIRCLE
public static PiercingInsertBuilder.PunchPocketTypeItemsPP valueOf(int value)
public static PiercingInsertBuilder.PunchPocketTypeItemsPP valueOf(String name)
public static PiercingInsertBuilder.PunchPocketTypeItemsPP[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.