public static class LsdynaGeometryPreparationBuilder.TargetBinder extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BINDER
For the process, the target of binder is binder.
|
static int |
_DIE
For the process, the target of binder is die.
|
static int |
_PUNCH
For the process, the target of binder is punch.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
BINDER
For the process, the target of binder is binder.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
DIE
For the process, the target of binder is die.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
PUNCH
For the process, the target of binder is punch.
|
Modifier and Type | Method and Description |
---|---|
static LsdynaGeometryPreparationBuilder.TargetBinder |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.TargetBinder |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.TargetBinder[] |
values()
Returns an array that contains the values for this enum.
|
public static final LsdynaGeometryPreparationBuilder.TargetBinder PUNCH
public static final LsdynaGeometryPreparationBuilder.TargetBinder BINDER
public static final LsdynaGeometryPreparationBuilder.TargetBinder DIE
public static final int _PUNCH
public static final int _BINDER
public static final int _DIE
public static LsdynaGeometryPreparationBuilder.TargetBinder valueOf(int value)
public static LsdynaGeometryPreparationBuilder.TargetBinder valueOf(String name)
public static LsdynaGeometryPreparationBuilder.TargetBinder[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.