public static class FormingInsertBuilder.BlankPositions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIE_PLATE
the blank is on the die plate
|
static int |
_PUNCH_PLATE
the blank is on the punch plate
|
static int |
_STRIPPER_PLATE
the blank is on the stripper plate
|
static FormingInsertBuilder.BlankPositions |
DIE_PLATE
the blank is on the die plate
|
static FormingInsertBuilder.BlankPositions |
PUNCH_PLATE
the blank is on the punch plate
|
static FormingInsertBuilder.BlankPositions |
STRIPPER_PLATE
the blank is on the stripper plate
|
Modifier and Type | Method and Description |
---|---|
static FormingInsertBuilder.BlankPositions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FormingInsertBuilder.BlankPositions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FormingInsertBuilder.BlankPositions[] |
values()
Returns an array that contains the values for this enum.
|
public static final FormingInsertBuilder.BlankPositions PUNCH_PLATE
public static final FormingInsertBuilder.BlankPositions STRIPPER_PLATE
public static final FormingInsertBuilder.BlankPositions DIE_PLATE
public static final int _PUNCH_PLATE
public static final int _STRIPPER_PLATE
public static final int _DIE_PLATE
public static FormingInsertBuilder.BlankPositions valueOf(int value)
public static FormingInsertBuilder.BlankPositions valueOf(String name)
public static FormingInsertBuilder.BlankPositions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.