Package | Description |
---|---|
nxopen.sim |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation.
|
Modifier and Type | Field and Description |
---|---|
static KinematicAxisBuilder.AxisMotionType |
KinematicAxisBuilder.AxisMotionType.LINEAR
linear axis
|
static KinematicAxisBuilder.AxisMotionType |
KinematicAxisBuilder.AxisMotionType.LINEAR_NC_AXIS
linear NC-axis
|
static KinematicAxisBuilder.AxisMotionType |
KinematicAxisBuilder.AxisMotionType.ROTARY
rotary axis
|
static KinematicAxisBuilder.AxisMotionType |
KinematicAxisBuilder.AxisMotionType.ROTARY_NC_AXIS
rotary NC-axis
|
Modifier and Type | Method and Description |
---|---|
KinematicAxisBuilder.AxisMotionType |
KinematicAxisBuilder.type()
Returns the axis motion
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
static KinematicAxisBuilder.AxisMotionType |
KinematicAxisBuilder.AxisMotionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static KinematicAxisBuilder.AxisMotionType |
KinematicAxisBuilder.AxisMotionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static KinematicAxisBuilder.AxisMotionType[] |
KinematicAxisBuilder.AxisMotionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
KinematicAxisBuilder.setType(KinematicAxisBuilder.AxisMotionType type)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.