Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static StockPartConverterBuilder.PartOption |
StockPartConverterBuilder.PartOption.WORK_PART
Upgrades stocks from the work part only
|
static StockPartConverterBuilder.PartOption |
StockPartConverterBuilder.PartOption.WORK_PART_WITH_LOADED_CHILDREN
Upgraded stocks from work part as well loaded children parts
|
Modifier and Type | Method and Description |
---|---|
StockPartConverterBuilder.PartOption |
StockPartConverterBuilder.convertWorkPartAndLoadedChildrenOption()
Returns the convert workpart and loaded children option.
|
static StockPartConverterBuilder.PartOption |
StockPartConverterBuilder.PartOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StockPartConverterBuilder.PartOption |
StockPartConverterBuilder.PartOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StockPartConverterBuilder.PartOption[] |
StockPartConverterBuilder.PartOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StockPartConverterBuilder.setConvertWorkPartAndLoadedChildrenOption(StockPartConverterBuilder.PartOption conversionOption)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.