Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
SplineSegment |
SBendCorner.SBendData.segment
S-Bend segment
|
Modifier and Type | Method and Description |
---|---|
SplineSegment |
SBendCorner.getSegment()
Gets the segment being used to represent the S-Bend.
|
Modifier and Type | Method and Description |
---|---|
boolean |
DiscontinuityCornerCollection.areSegmentsDisconnected(SplineSegment segment1,
SplineSegment segment2,
ControlPoint rcp)
Checks whether segment1 and segment2 are disconnected at a control point
due to a discontinuity corner.
|
SBendCorner |
SBendCornerCollection.createCornerBySegBendRadius(ControlPoint startRcp,
ControlPoint endRcp,
SplineSegment segment,
int sbendType,
double bendRadius)
Creates a S-Bend corner between the start rcp and end rcp using a
SplineSegment and a bend radius. |
SBendCorner |
SBendCornerCollection.createCornerBySegBendRatio(ControlPoint startRcp,
ControlPoint endRcp,
SplineSegment segment,
int sbendType,
double bendRatio)
Creates a S-Bend corner between the start rcp and end rcp using a
SplineSegment and a bend ratio. |
SBendCorner |
SBendCornerCollection.getSBendAssociatedToSegment(SplineSegment segment)
Enquire the S-Bend Corner that this segment represents.
|
double |
SBendCornerCollection.getSegmentSBendRadius(SplineSegment segment)
Gets the bend radius of a segment associated S-Bend corner.
|
void |
SBendCorner.setSBendData(int sbendType,
ControlPoint startRcp,
ControlPoint endRcp,
SplineSegment segment,
double radiusOrRatio,
boolean useBendRatio)
Set the data for the S-Bend object
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.