Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static SplinePathBuilder.SplinePathAttributeOptions |
SplinePathBuilder.SplinePathAttributeOptions.RADIUS
A radius method option for spline user attribute
|
static SplinePathBuilder.SplinePathAttributeOptions |
SplinePathBuilder.SplinePathAttributeOptions.RATIO_TO_DIAMETER
A ratio to diameter method option for spline user attribute
|
Modifier and Type | Method and Description |
---|---|
SplinePathBuilder.SplinePathAttributeOptions |
SplinePathBuilder.minimumCheckingMethod()
Returns the minimum checking method for this spline.
|
static SplinePathBuilder.SplinePathAttributeOptions |
SplinePathBuilder.SplinePathAttributeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplinePathBuilder.SplinePathAttributeOptions |
SplinePathBuilder.SplinePathAttributeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplinePathBuilder.SplinePathAttributeOptions[] |
SplinePathBuilder.SplinePathAttributeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SplinePathBuilder.setMinimumCheckingMethod(SplinePathBuilder.SplinePathAttributeOptions routeCheckingMethod)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.