Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static Run.FlipStatus |
Run.FlipStatus.CANNOT_FLIP
Run is deleted or there are no segments attached to component.
|
static Run.FlipStatus |
Run.FlipStatus.FLOW_TYPE_MISMATCH
Ports are defined with ambiguous flow types.
|
static Run.FlipStatus |
Run.FlipStatus.FOLLOWS_FLOW
Ports correctly aligned with flow.
|
static Run.FlipStatus |
Run.FlipStatus.NOT_TWO_PORTS
Given component ports are not equal to two ports.
|
static Run.FlipStatus |
Run.FlipStatus.PORT_POSITION_MISMATCH
Ports are not collinear and opposite or perpendicular.
|
static Run.FlipStatus |
Run.FlipStatus.RUN_FLOW_NOT_DEFINED
Flow is not defined on Run.
|
static Run.FlipStatus |
Run.FlipStatus.SUCCESS
Component is flipped.
|
static Run.FlipStatus |
Run.FlipStatus.UNEQUAL_CONSTRAINTS
Each ports has different number of constraints.
|
Modifier and Type | Method and Description |
---|---|
Run.FlipStatus |
Run.flipComponent(Component component)
Flips a component that is part of a run by rotating the component so that it's input and output ports reverse.
|
static Run.FlipStatus |
Run.FlipStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Run.FlipStatus |
Run.FlipStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Run.FlipStatus[] |
Run.FlipStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.