Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static PointDefinition |
PointDefinition.END
The point defines the end of the overstock application.
|
static PointDefinition |
PointDefinition.MIDDLE
The point defines the middle of the overstock application.
|
static PointDefinition |
PointDefinition.START
The point defines the start of the overstock application.
|
Modifier and Type | Method and Description |
---|---|
static PointDefinition |
PointDefinition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointDefinition |
PointDefinition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointDefinition[] |
PointDefinition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
OverstockApplication |
OverstockApplicationCollection.convertOverstockApplication(ControlPoint startControlPoint,
ISegment[] segments,
Stock[] stocks,
Point definingPoint,
PointDefinition definingDirection,
Expression pieceLength,
CharacteristicList overstockPart,
CharacteristicList reqOptCharxList,
Expression wrapValue,
Overstock[] overstocks)
Converts an existing
Overstock to
Routing.Method#POINT_AND_LENGTH overstock. |
OverstockApplication |
OverstockApplicationCollection.createOverstockApplication(ControlPoint startControlPoint,
ISegment[] segments,
Stock[] stocks,
Point definingPoint,
PointDefinition definingDirection,
Expression pieceLength,
CharacteristicList overstockPart,
WrapApplicationType stockWrapType,
Expression wrapValue)
Creates the
Routing.Method#POINT_AND_LENGTH
overstock by the Point and Length method. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.