Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static OverstockBuilder.ApplicationType |
OverstockBuilder.ApplicationType.ENTIRE_SEGMENTS
Entire Segments
|
static OverstockBuilder.ApplicationType |
OverstockBuilder.ApplicationType.INTERVAL
Interval
|
static OverstockBuilder.ApplicationType |
OverstockBuilder.ApplicationType.POINT_AND_LENGTH
Point And Length
|
static OverstockBuilder.ApplicationType |
OverstockBuilder.ApplicationType.POINT_TO_POINT
Point To Point
|
Modifier and Type | Method and Description |
---|---|
OverstockBuilder.ApplicationType |
OverstockBuilder.applicationMethod()
Returns the application method for overstock assignment.
|
static OverstockBuilder.ApplicationType |
OverstockBuilder.ApplicationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OverstockBuilder.ApplicationType |
OverstockBuilder.ApplicationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OverstockBuilder.ApplicationType[] |
OverstockBuilder.ApplicationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OverstockBuilder.setApplicationMethod(OverstockBuilder.ApplicationType applicationMethod)
License requirements: routing_advanced ("Routing Advanced") OR routing_harness ("Routing Harness") OR routing_cabling ("Routing Cabling") OR routing_pipetube ("Routing Piping and Tubing") OR routing_hvac ("Routing HVAC") OR routing_platform ("Routing Platform") OR routing_pid ("Routing PID") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.