Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Component
Represents a component in a
ComponentAssembly . |
interface |
ExplodedComponent
Represents a
Component within an explosion. |
Modifier and Type | Interface and Description |
---|---|
interface |
Anchor
A Routing Anchor defines a position in a Qualified Routing component part.
|
interface |
ArcSegment
Represents a arc segment.
|
interface |
AssemblyDefinition
Represents a collection of
SingleDevice objects that are used in an assembled product. |
interface |
BuiltInPath
The Routing BuiltInPath object stores a set of curves.
|
interface |
ConnectivityDefinition
The base class for various connection objects.
|
interface |
ControlPoint
Routing Control Points define a position in space, and are used to determine connections
from segments to segments, and segments to ports.
|
interface |
CrossSection
A
CrossSection defines a profile to sweep for Stock objects. |
interface |
Filler
Represents a Filler .
|
interface |
FittingOverstock
The
FittingOverstock object represents overstock
applied over the faces of the routing parts. |
interface |
GapArcSegment
Represents a gap arc segment.
|
interface |
InterfaceTerminalBase
The
InterfaceTerminalBase corresponds to an abstract class for
a prototype nxopen.routing.Port . |
interface |
InterfaceTerminalShadow
Represents the defining data for a physical
nxopen.routing.Port . |
interface |
IRoutePosition
Interface class for all routing objects that specify a single (possibly associative) location
in space.
|
interface |
ISegment
Interface class for all routing segments [Line/Arc/Spline] .
|
interface |
ItemDefinition
ItemDefinition object corresponds to DDID in AP212 and to a piece
part or routing stock in NX. |
interface |
LineSegment
Represents a line segment.
|
interface |
LogicalTerminal
Assembly instance of a
InterfaceTerminalBase . |
interface |
Overstock
Represents an
Overstock object. |
interface |
PartDefinitionBase
The abstract class
PartDefinitionBase contains
information defining a logical part. |
interface |
PartDefinitionShadow
PartDefinitionShadow contains the defining data for a
logical part, such as an connector. |
interface |
RouteObject
The Top level routing data model object.
|
interface |
SingleDevice
The Routing SingleDevice corresponds to an abstract instance of
ItemDefinition . |
interface |
SplineSegment
Represents a spline segment.
|
interface |
Stock
The
Stock object represents a material (such as as pipe or tube)
that covers a path of segments. |
interface |
StockData
|
interface |
StockDefinition
Represents Routing StockDefinition object
Creator not available in KF. |
interface |
StockDevice
The Routing StockDevice corresponds to a generic stock instance
of
Routing.SingleDevice . |
interface |
StockTransition
Represents
StockTransition object. |
Modifier and Type | Interface and Description |
---|---|
interface |
CableDefinition
Holds the collection of wires in a
CableDevice . |
interface |
CableDevice
Corresponds to a cable instance of an
ElectricalStockDevice . |
interface |
CableStockDefinition
Describes a cable's stock.
|
interface |
ConnectorDevice
The Electrical ConnectorDevice corresponds to a connector instance of
SingleDevice . |
interface |
ElectricalPartDefinitionShadow
Represents
ElectricalPartDefinitionShadow object Creator not available in KF. |
interface |
ElectricalStockDefinition
Represents
ElectricalStockDefinition object Creator not available in KF. |
interface |
ElectricalStockDevice
The Electrical Stock Device is a non instantiable superclass to classify
all electrical stock-based single devices.
|
interface |
HarnessDefinition
Represents a
HarnessDefinition Creator not available in KF. |
interface |
HarnessDevice
The Electrical HarnessDevice corresponds to a harness instance of the
Routing.SingleDevice . |
interface |
ShieldDefinition
Represents Routing Electrical ShieldDefinition object
Creator not available in KF. |
interface |
ShieldDevice
The Electrical ShieldDevice corresponds to a shield instance of
Routing.Electrical.ElectricalStockDevice . |
interface |
ShieldStockDefinition
Represents Routing Electrical ShieldStockDefinition object
Creator not available in KF. |
interface |
SystemDefinition
Represents a
SystemDefinition Creator not available in KF. |
interface |
SystemDevice
The Electrical SystemDevice corresponds to a system instance of the
SingleDevice . |
interface |
WireDevice
The Electrical WireDevice corresponds to a wire instance of
ElectricalStockDevice . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.