Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static FittingOverstockBuilder.TrimMethod |
FittingOverstockBuilder.TrimMethod.BETWEEN_PLANES
Double Trim Planes
|
static FittingOverstockBuilder.TrimMethod |
FittingOverstockBuilder.TrimMethod.TRIM_PLANE
Single Trim Plane
|
Modifier and Type | Method and Description |
---|---|
FittingOverstockBuilder.TrimMethod |
FittingOverstockBuilder.faceTrimMethod()
Returns the
FittingOverstockBuilder.TrimMethod
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") Created in NX7.5.0 |
static FittingOverstockBuilder.TrimMethod |
FittingOverstockBuilder.TrimMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FittingOverstockBuilder.TrimMethod |
FittingOverstockBuilder.TrimMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FittingOverstockBuilder.TrimMethod[] |
FittingOverstockBuilder.TrimMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FittingOverstockBuilder.setFaceTrimMethod(FittingOverstockBuilder.TrimMethod faceTrimMethod)
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.