Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static CornerTypeBuilder.BendMethods |
CornerTypeBuilder.BendMethods.BEND_RADIUS_TABLE
Bend table method creates bend from specified bend table
|
static CornerTypeBuilder.BendMethods |
CornerTypeBuilder.BendMethods.INNER_RADIUS
Inner Radius method allows corner creation with the specified inner radius value
|
static CornerTypeBuilder.BendMethods |
CornerTypeBuilder.BendMethods.RADIUS
Radius method allows corner creation with the specified radius value
|
static CornerTypeBuilder.BendMethods |
CornerTypeBuilder.BendMethods.RATIO_TO_DIAMETER
Ratio to diameter method
|
Modifier and Type | Method and Description |
---|---|
CornerTypeBuilder.BendMethods |
BendCorner.bendMethod()
Returns the bend method
License requirements: routing_base ("Routing Basic") . |
CornerTypeBuilder.BendMethods |
CornerTypeBuilder.routeCornerBendMethods()
Returns the route corner bend options
License requirements: routing_base ("Routing Basic") . |
static CornerTypeBuilder.BendMethods |
CornerTypeBuilder.BendMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CornerTypeBuilder.BendMethods |
CornerTypeBuilder.BendMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CornerTypeBuilder.BendMethods[] |
CornerTypeBuilder.BendMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
BendCorner |
BendCornerCollection.createCorner(ControlPoint rcp,
CornerTypeBuilder.BendMethods bendMethod,
double bendRatio,
double bendRadius)
Create a bend corner object at a Control Point.
|
void |
BendCorner.setBendMethod(CornerTypeBuilder.BendMethods bendMethod)
Sets the bend method
License requirements: routing_base ("Routing Basic") . |
void |
CornerTypeBuilder.setRouteCornerBendMethods(CornerTypeBuilder.BendMethods routeCornerBendMethods)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.