Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static ConvertLinearToEccentricLinear |
ConvertLinearToEccentricLinear.CONVERTED
Is converted linear to Eccentric linear
|
static ConvertLinearToEccentricLinear |
ConvertLinearToEccentricLinear.NOT_CONVERTED
Is not converted linear to Eccentric linear
|
Modifier and Type | Method and Description |
---|---|
ConvertLinearToEccentricLinear |
ISegment.convertLinearToEccentricLinear()
Is line segment converted to eccentric line segment?
|
static ConvertLinearToEccentricLinear |
ConvertLinearToEccentricLinear.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConvertLinearToEccentricLinear |
ConvertLinearToEccentricLinear.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConvertLinearToEccentricLinear[] |
ConvertLinearToEccentricLinear.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.