Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static ConvertEccentricLinearToLinear |
ConvertEccentricLinearToLinear.CONVERTED
Is converted Eccentric linear to linear
|
static ConvertEccentricLinearToLinear |
ConvertEccentricLinearToLinear.NOT_CONVERTED
Is not converted Eccentric linear to linear
|
Modifier and Type | Method and Description |
---|---|
ConvertEccentricLinearToLinear |
ISegment.convertEccentricLinearToLinear()
Is line segment eccentric converted to line segment?
|
static ConvertEccentricLinearToLinear |
ConvertEccentricLinearToLinear.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConvertEccentricLinearToLinear |
ConvertEccentricLinearToLinear.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConvertEccentricLinearToLinear[] |
ConvertEccentricLinearToLinear.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.