public class WrapApplicationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_GAPPED
Barber pole spiral wrap application, e.g., no overlap
|
static int |
_OVERLAPPED
Overlapping spiral wrap application, e.g., [0-100)% overlap
|
static int |
_SPOT
Spot wrap application, i.e., 100% overlap
|
static int |
_UNKNOWN
Unknown wrap application
|
static WrapApplicationType |
GAPPED
Barber pole spiral wrap application, e.g., no overlap
|
static WrapApplicationType |
OVERLAPPED
Overlapping spiral wrap application, e.g., [0-100)% overlap
|
static WrapApplicationType |
SPOT
Spot wrap application, i.e., 100% overlap
|
static WrapApplicationType |
UNKNOWN
Unknown wrap application
|
Modifier and Type | Method and Description |
---|---|
static WrapApplicationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WrapApplicationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WrapApplicationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final WrapApplicationType UNKNOWN
public static final WrapApplicationType SPOT
public static final WrapApplicationType OVERLAPPED
public static final WrapApplicationType GAPPED
public static final int _UNKNOWN
public static final int _SPOT
public static final int _OVERLAPPED
public static final int _GAPPED
public static WrapApplicationType valueOf(int value)
public static WrapApplicationType valueOf(String name)
public static WrapApplicationType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.