public interface StockOffsetPointBuilder extends Builder
Point
or
ControlPoint
to mimic the update/move behavior of
the input smart Point
. The smart point may be a Routing
stock offset point (see PointCollection.createStockOffsetPoint(nxopen.Point, Direction, java.lang.String, nxopen.SmartObject.UpdateOption)
) or
any of the points created using the PointCollection
class.
RouteManager.createStockOffsetPointBuilder(nxopen.NXObject)
Modifier and Type | Interface and Description |
---|---|
static class |
StockOffsetPointBuilder.PointData
This class holds the data returned from
getPointData() |
static class |
StockOffsetPointBuilder.PointType
Point Type
|
Modifier and Type | Method and Description |
---|---|
Point |
constraintPoint()
Returns the point that defines the location of the selected point.
|
StockOffsetPointBuilder.PointData |
getPointData()
Gets the stock offset data from the currently selected point or routing
control point.
|
SelectNXObject |
pointSelection()
Returns the point selection.
|
void |
setConstraintPoint(Point point)
Sets the point that defines the location of the selected point.
|
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectNXObject pointSelection() throws NXException, RemoteException
NXException
RemoteException
StockOffsetPointBuilder.PointData getPointData() throws NXException, RemoteException
NXException
RemoteException
Point constraintPoint() throws NXException, RemoteException
NXException
RemoteException
void setConstraintPoint(Point point) throws NXException, RemoteException
point
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.