public static class Run.Status extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BROKEN
Run is broken.
|
static int |
_INCOMPLETE
Run is incomplete.
|
static int |
_VALID
Run is valid.
|
static Run.Status |
BROKEN
Run is broken.
|
static Run.Status |
INCOMPLETE
Run is incomplete.
|
static Run.Status |
VALID
Run is valid.
|
Modifier and Type | Method and Description |
---|---|
static Run.Status |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Run.Status |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Run.Status[] |
values()
Returns an array that contains the values for this enum.
|
public static final Run.Status VALID
public static final Run.Status BROKEN
public static final Run.Status INCOMPLETE
public static final int _VALID
public static final int _BROKEN
public static final int _INCOMPLETE
public static Run.Status valueOf(int value)
public static Run.Status valueOf(String name)
public static Run.Status[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.