public static class RouteManager.ImportMode extends Enum
++--------------+---------------+-----------------+ +------------+------------++ Deletes | Replaces data | Preserves | | | Import || unmatched | in matching | existing | | ImportMode | File Type || elements | elements | connectors | +============+============++==============+===============+=================+ | Update | XML || Yes | Yes | No | | | Legacy CMP || No | Yes | Yes | | | Legacy HRN || Yes(1) | Yes(2) | Yes | +------------+------------++--------------+---------------+-----------------+ | Merge | XML || No | Yes | Yes | | | Legacy CMP || No | Yes | Yes | | | Legacy HRN || No | Yes(2) | Yes | +------------+------------++--------------+---------------+-----------------+ | Append | XML || No | No | Yes | | | Legacy CMP || No | No | Yes | | | Legacy HRN || No | No | Yes | +------------+------------++--------------+---------------+-----------------+ ++--------------+---------------+-----------------+------------------+ +------------+------------++ May add new | May add new | May create | May create | | | Import || connectors | connections | duplicate | duplicate | | ImportMode | File Type || | | connector names | connection names | +============+============++==============+===============+=================+==================+ | Update | XML || Yes | Yes | Yes(3) | Yes(3) | | | Legacy CMP || Yes | No | No | No | | | Legacy HRN || Yes | Yes | No | No | +------------+------------++--------------+---------------+-----------------+------------------+ | Merge | XML || Yes | Yes | Yes(3) | Yes(3) | | | Legacy CMP || Yes | No | No | No | | | Legacy HRN || Yes | Yes | No | No | +------------+------------++--------------+---------------+-----------------+------------------+ | Append | XML || Yes | Yes | Yes | Yes | | | Legacy CMP || Yes | No | Yes | No | | | Legacy HRN || Yes | Yes | No | Yes | +------------+------------++--------------+---------------+-----------------+------------------+ ++--------------+---------------+-----------------+ || Maintains | Maintains | Elements | || assignment | routing | matching | +------------+------------++ information | information | criterion | | | Import || for matching | for matching | | | ImportMode | File Type || connectors | connections | | +============+============++==============+===============+=================+ | Update | XML || Yes | Yes | GUID | | | Legacy CMP || Yes | Yes | Names(4) | | | Legacy HRN || Yes | Yes | Names(4) | +------------+------------++--------------+---------------+-----------------+ | Merge | XML || Yes | Yes | GUID | | | Legacy CMP || Yes | Yes | Names(4) | | | Legacy HRN || Yes | Yes | Names(4) | +------------+------------++--------------+---------------+-----------------+ | Append | XML || No | No | N/A | | | Legacy CMP || No | No | N/A | | | Legacy HRN || No | No | N/A | +------------+------------++--------------+---------------+-----------------+
Modifier and Type | Field and Description |
---|---|
static int |
_APPEND
Create the imported objects as new objects.
|
static int |
_MERGE
Update existing objects with data from the imported objects.
|
static int |
_UPDATE
Update existing objects with data from the imported objects.
|
static RouteManager.ImportMode |
APPEND
Create the imported objects as new objects.
|
static RouteManager.ImportMode |
MERGE
Update existing objects with data from the imported objects.
|
static RouteManager.ImportMode |
UPDATE
Update existing objects with data from the imported objects.
|
Modifier and Type | Method and Description |
---|---|
static RouteManager.ImportMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RouteManager.ImportMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RouteManager.ImportMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final RouteManager.ImportMode UPDATE
public static final RouteManager.ImportMode MERGE
public static final RouteManager.ImportMode APPEND
public static final int _UPDATE
public static final int _MERGE
public static final int _APPEND
public static RouteManager.ImportMode valueOf(int value)
public static RouteManager.ImportMode valueOf(String name)
public static RouteManager.ImportMode[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.