public interface FormboardFrameCollection extends TaggedObjectCollection
FormboardFrame
objects. RouteManager
Modifier and Type | Interface and Description |
---|---|
static class |
FormboardFrameCollection.ImportPatternData
This class holds the data returned from
importPattern(java.lang.String, int, java.lang.String) |
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
FormboardFrame |
createFormboardFrameByRectangle(Point point,
Scalar height,
Scalar width)
Creates a
FormboardFrame object
using a rectangle defined by a Point object and
two Scalar objects that represent the height and width. |
FormboardFrameCollection.ImportPatternData |
importPattern(String filename,
int type,
String frameName)
Creates a
FormboardFrame object by
importing formboard frame pattern
License requirements: routing_harness ("Routing Harness") Created in NX5.0.0 |
_find_next, iterator
FormboardFrame createFormboardFrameByRectangle(Point point, Scalar height, Scalar width) throws NXException, RemoteException
FormboardFrame
object
using a rectangle defined by a Point
object and
two Scalar
objects that represent the height and width.
point
- Lower left cornerheight
- width
- NXException
RemoteException
FormboardFrameCollection.ImportPatternData importPattern(String filename, int type, String frameName) throws NXException, RemoteException
FormboardFrame
object by
importing formboard frame pattern
filename
- Filename of the file to be imported type
- Type of file importedframeName
- new name of frame NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.