Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Method and Description |
---|---|
ReferenceSetBehavior |
ViewStyleInheritPmiBuilder.referenceSetBehavior()
Returns the reference set option
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ViewStyleInheritPmiBuilder.setReferenceSetBehavior(ReferenceSetBehavior pmiOption)
License requirements: drafting ("DRAFTING") . |
Modifier and Type | Field and Description |
---|---|
static ReferenceSetBehavior |
ReferenceSetBehavior.ALL
Inherit all PMI regardless of whether the referenced objects are in the active reference set.
|
static ReferenceSetBehavior |
ReferenceSetBehavior.NONE
No PMI will be inherited if any of the PMI objects has a reference to an object which is not in the active reference set.
|
static ReferenceSetBehavior |
ReferenceSetBehavior.PARTIAL
Inherit only PMI for which all of the referenced objects are in the active reference set.
|
Modifier and Type | Method and Description |
---|---|
static ReferenceSetBehavior |
ReferenceSetBehavior.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReferenceSetBehavior |
ReferenceSetBehavior.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReferenceSetBehavior[] |
ReferenceSetBehavior.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.