public static class SessionSketch.BackgroundType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INHERIT
Sketch background color is inherited from the parent application
|
static int |
_PLAIN
Sketch background color is forced to the plain background color
|
static SessionSketch.BackgroundType |
INHERIT
Sketch background color is inherited from the parent application
|
static SessionSketch.BackgroundType |
PLAIN
Sketch background color is forced to the plain background color
|
Modifier and Type | Method and Description |
---|---|
static SessionSketch.BackgroundType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionSketch.BackgroundType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionSketch.BackgroundType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionSketch.BackgroundType INHERIT
public static final SessionSketch.BackgroundType PLAIN
public static final int _INHERIT
public static final int _PLAIN
public static SessionSketch.BackgroundType valueOf(int value)
public static SessionSketch.BackgroundType valueOf(String name)
public static SessionSketch.BackgroundType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.