public static class SessionModeling.SaveDataForFeatureEditOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FAST_ROLLBACK
Indicates the additional parasolid data is saved for faster rollback
|
static int |
_FAST_ROLLBACK_AND_PREVIOUS_STATE_OF_FAILED_FEATURE
Indicates the additional parasolid data is saved for faster rollback and to show the previous state of failed feature
|
static int |
_NONE
Indicates the no additional data is saved
|
static SessionModeling.SaveDataForFeatureEditOption |
FAST_ROLLBACK
Indicates the additional parasolid data is saved for faster rollback
|
static SessionModeling.SaveDataForFeatureEditOption |
FAST_ROLLBACK_AND_PREVIOUS_STATE_OF_FAILED_FEATURE
Indicates the additional parasolid data is saved for faster rollback and to show the previous state of failed feature
|
static SessionModeling.SaveDataForFeatureEditOption |
NONE
Indicates the no additional data is saved
|
Modifier and Type | Method and Description |
---|---|
static SessionModeling.SaveDataForFeatureEditOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.SaveDataForFeatureEditOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.SaveDataForFeatureEditOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionModeling.SaveDataForFeatureEditOption NONE
public static final SessionModeling.SaveDataForFeatureEditOption FAST_ROLLBACK
public static final SessionModeling.SaveDataForFeatureEditOption FAST_ROLLBACK_AND_PREVIOUS_STATE_OF_FAILED_FEATURE
public static final int _NONE
public static final int _FAST_ROLLBACK
public static final int _FAST_ROLLBACK_AND_PREVIOUS_STATE_OF_FAILED_FEATURE
public static SessionModeling.SaveDataForFeatureEditOption valueOf(int value)
public static SessionModeling.SaveDataForFeatureEditOption valueOf(String name)
public static SessionModeling.SaveDataForFeatureEditOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.