Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.pdm |
Provides classes and interfaces for PDM.
|
Modifier and Type | Method and Description |
---|---|
LogicalObject[] |
DesignElementBuilder.createLogicalObjects()
Creates the pre-creation objects for the design elements
License requirements: nx_4gd_integration ("4th Generation Design") . |
Modifier and Type | Method and Description |
---|---|
LogicalObject[] |
CopyPasteNewBuilder.createLogicalObjects()
Creates the pre-creation logical objects
License requirements: nx_ship_detail ("Ship Detail Design") . |
Modifier and Type | Interface and Description |
---|---|
interface |
NativePartLogicalObject
Represents the class that contains information for the objects participating in import operation.
|
Modifier and Type | Method and Description |
---|---|
LogicalObject[] |
PartOperationBuilder.createLogicalObjects()
Creates the pre-creation objects for the parts
License requirements: None. |
LogicalObject[] |
ObjectCreateBuilder.createLogicalObjects()
Creates Pre-Creation LogicalObjects
License requirements: None. |
LogicalObject |
PartOperationAttributePropertiesBuilder.referenceObject()
Returns the referenced logical object from this attribute.
|
Modifier and Type | Method and Description |
---|---|
void |
PartOperationCopyBuilder.createNonMasterListForCopyLogicalObject(LogicalObject logicalObject)
Create NonMaster list for the selected logical Object
License requirements: None. |
void |
PartOperationBuilder.createNonMasterListForLogicalObject(LogicalObject logicalObject)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder.createNonMasterListForCopyLogicalObject(nxopen.pdm.LogicalObject) instead
|
void |
PartOperationBuilder.createSpecificationsForLogicalObjects(LogicalObject[] logicalObjects)
Create new specifications for Logical Objects
License requirements: None. |
boolean |
PartOperationBuilder.editNonMasterName(LogicalObject logicalObject,
String oldName,
String newName)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder.editNonMasterToCopyName(nxopen.pdm.LogicalObject, java.lang.String, java.lang.String) instead
|
boolean |
PartOperationCopyBuilder.editNonMasterToCopyName(LogicalObject logicalObject,
String oldName,
String newName)
Sets the name the non-master part will get saved as.
|
AlternateIdManager |
PartOperationBuilder.getAlternateIDManager(LogicalObject logicalObject)
Create an instance of a
AlternateIdManager
class that will be used to create alternate ID information while creating the new part. |
PartOperationCopyBuilder.CopyNonMasterParts |
PartOperationCopyBuilder.getCopyNonMasterPartsOption(LogicalObject logicalObject)
Get the nonmasters saveAs option for given logical object.
|
PartOperationBuilder.NonMasterSaveAs |
PartOperationBuilder.getNonMasterCopyOption(LogicalObject logicalObject)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder.getCopyNonMasterPartsOption(nxopen.pdm.LogicalObject) instead
|
String[] |
PartOperationBuilder.getNonMasterList(LogicalObject logicalObject)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder.getNonMasterListForCopyLogicalObject(nxopen.pdm.LogicalObject) instead
|
String[] |
PartOperationCopyBuilder.getNonMasterListForCopyLogicalObject(LogicalObject logicalObject)
Gets NonMaster list for the given logical Object
License requirements: None. |
boolean |
PartOperationBuilder.isNonMasterBeingCopied(LogicalObject logicalObject,
String partName)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder.isNonMasterForLogicalObjectBeingCopied(nxopen.pdm.LogicalObject, java.lang.String) instead
|
boolean |
PartOperationCopyBuilder.isNonMasterForLogicalObjectBeingCopied(LogicalObject logicalObject,
String partName)
Returns whether or not the non-master part specified for the given
LogicalObject will actually
get saved during the save as operation. |
void |
PartOperationCopyBuilder.setCopyNonMasterPartsOption(LogicalObject logicalObject,
PartOperationCopyBuilder.CopyNonMasterParts saveOption)
Set the nonmasters saveAs option for given logical object.
|
void |
PartOperationBuilder.setNonMasterSaveAsOption(LogicalObject logicalObject,
PartOperationBuilder.NonMasterSaveAs saveOption)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder.setCopyNonMasterPartsOption(nxopen.pdm.LogicalObject, nxopen.pdm.PartOperationCopyBuilder.CopyNonMasterParts) instead
|
void |
PartOperationAttributePropertiesBuilder.setReferenceObject(LogicalObject referencedLogicalObject)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
PartOperationCopyBuilder.setSelectedNonMasterToCopy(LogicalObject logicalObject,
String partName)
Sets whether or not the non-master part specified will actually
get saved during the save as operation.
|
void |
PartOperationBuilder.setSelectedNonMasterToSaveAs(LogicalObject logicalObject,
String partName)
Deprecated.
Deprecated in NX10.0.0. Use
PartOperationCopyBuilder.setSelectedNonMasterToCopy(nxopen.pdm.LogicalObject, java.lang.String) instead
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.