Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PackagingTraceBuilder.Frame |
PackagingTraceBuilder.Frame.ABSOLUTE
Traced copies positioned in absolute coordinate system.
|
static PackagingTraceBuilder.Frame |
PackagingTraceBuilder.Frame.RELATIVE
Traced copies positioned relative to selected links.
|
Modifier and Type | Method and Description |
---|---|
PackagingTraceBuilder.Frame |
PackagingTraceBuilder.frameType()
Returns the
PackagingTrace reference frame type
defined at PackagingTraceBuilder.Frame
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
static PackagingTraceBuilder.Frame |
PackagingTraceBuilder.Frame.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PackagingTraceBuilder.Frame |
PackagingTraceBuilder.Frame.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PackagingTraceBuilder.Frame[] |
PackagingTraceBuilder.Frame.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PackagingTraceBuilder.setFrameType(PackagingTraceBuilder.Frame fType)
Sets the
PackagingTrace reference frame type
defined at PackagingTraceBuilder.Frame
License requirements: mechanisms ("MECHANISMS") Created in NX4.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.